Technical FAQs

Ask a Question

Can I install Unitypro V11 on Disk D?

You can install Unity Pro V11 on your disk.
But if the PC runs on Windows 8 or higher, you must follow this installation procedure:
1. Launch regedit.exe
2. Go on the following path : HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\FileSystem
3. Modify the key NtfsDisable8dot3NameCreation : set its value to 0
4. Install Unity Pro V11.0
Was this helpful?
What can we do to improve the information ?