Technical FAQs

Ask a Question

Will Vijeo Designer resize the panels when going from higher to lower resolution screens?

Vijeo Designer will not automatically resize a larger screen to a smaller one.  This can be addressed by resizing the panels manually one by one.  ​To resize, go to the panel, select all of the objects and grab the corners of the outer dotted line to resize the objects to fit the panel.  This will need to be repeated for all of the panel pages.
 
Was this helpful?
What can we do to improve the information ?