Technical FAQs

Ask a Question

Osisense XC - What is the adapted head ZCKD06SC6

The adapted head ZCKD06SC6 is similar to the adapted ZCKD06S70 head, associated to the complete switch XCKL106S70. The ZCKD06S70 head is a special cat'whister rod (dia 1.2mm) of 300mm lenght with a dia 40mm buckle at the extremity to detect aircraft during refueling in the airport. The ZCKD06SC6 head is a special rod (dia 1.5mm) of 500mm lenght with a dia 40mm buckle at the extremity. Attached picture of this special rod head. The head ZCKD06SC6 is available to order in 2016 without any customer restriction, it is produced at order reception (not in stock).

Was this helpful?
What can we do to improve the information ?