Technical FAQs

Ask a Question

Osisense XC - Maximum temperature in operation of the ZCKJ18 contact body

What is the ZCKJ18 contact body in the XCKJ series : it is a ZCKJ1 contact body with gold flashed contacts instead of silver ones. It uses the XE2SP2158 gold flashed contact block, instead of the XE2SP2151 snap action contacts 2-pole NC+NO. Attached the ZCKJ18 data sheet confirming the temperature range in operation : -40°C ... +120°C. Available to order in 2016 (logistic ref ZCKJ18AC).
Be careful, when using gold flashed contacts, the switching power must be limited to avoid any gold flash destruction : 48V/10mA maxi (catalogue limitation in the general pages).
Was this helpful?
What can we do to improve the information ?