Technical FAQs

Ask a Question

On Lexium 32 is it possible to change the AT_Gain parameter?

Yes,  it is possible to modify the AT_gain

AT_Gain has a modbus address of 12052 and can be written to via the fieldbus.
It should be noted that AT_Gain is internally linked to the parameter Global_gain (MB4394).

During autotuning process At_gain displays the result of autotuning. The value 100% corresponds to the theoretical optimum .

Both parameters are coupled .
If you increase Globalgain then AT_gain increases also.

Was this helpful?
What can we do to improve the information ?