Technical FAQs

Ask a Question

What is the replacement part number for the gearbox with part number of GBX080005S853L ?

The gearbox with part number of GBX080005S853L is replaced by the following part numbers.

GBX080005K = 80mm planetary gearbox with 5:1 ratio
GBK0800853S = Adapter kit for mounting 80mm gearbox to motor with 85mm front flange and 14mm output shaft.

Please note that now there are two part numbers which are needed to duplicate the single part number of GBX080005S853L.
This is because Schneider Electric has separated the gearbox from the mounting plate which is used to affix the gearbox to the motor. 
Was this helpful?
What can we do to improve the information ?