Technical FAQs

Ask a Question

Osisense XS - Certifications of the adapted XS630B1PAM12TF proximity sensor -40°C in operation

Attached the XS630B1PAM12TF label on the product, giving the certifications of this special version TF (low temperature -40°C in operation), and the country of origin in 2016 :
- CE
- UL
- CSA
- CCC
- E2.

 
Was this helpful?
What can we do to improve the information ?