Technical FAQs

Ask a Question

Osisense XC special - Certifications of the XCRE181TG special version low temperature and protection against internal condensation

Attached the XCRE181TG marking on the product, giving the certifications of this special version TG (low temperature -40°C and protection against internal condensation) for ski lifts, and the country of origin in 2016 :
- CE
- CSA
- EAC
Was this helpful?
What can we do to improve the information ?