Technical FAQs

Ask a Question

Osisense XC - Is the special head ZCKD06S70 sold in spare parts ?

The special head ZCKD06S70 is not sold separately. It belongs to the adapted complete limit switch XCKL106S70 using ZCKL1 contact body. The ZCKD06S70 head is a special cat'whister rod of 300mm lenght with a buckle at the extremity to detect aircraft during refueling in the airport. Attached picture of the complete switch
2016 logistic information of the complete switch XCKL106S70 : available for all customers (no restriction), manufactured to order product, production in France.

Was this helpful?
What can we do to improve the information ?