Technical FAQs

Ask a Question

Will the Lexium 32 memory card, part number VW3M8705, work in a M241/251 controller?

Issue:
Will the Lexium 32 memory card, part number VW3M8705, work in a M241/251 controller?

Product Line:
TM241, TM251, Lexium32, SD card

Environment:


Cause:


Resolution:
The Lexium32 memory card is a SIM card where as the M241/M251 uses SD.  They are two different types of memory cards and will not work.
 
Was this helpful?
What can we do to improve the information ?