Technical FAQs

Ask a Question

ION EEM - Changing Trend Analysis Calendar Selector

Issue:
The calendar selector for the Fixed Date time range in the Trend Analysis has Monday as the left most day as opposed to Sunday. 



Product Line:
ION EEM 5.0

Environment:
Trend Analysis

Resolution:
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

1) On the ION EEM server, navigate to the \Schneider Electric\IONEEM\Web\EEMWeb\controls\ folder and open the InputDateRangeForTrend.ascx file in Notepad. 
2) There are two instances of firstDay: 1, in the file. The 1 represents Monday. Setting this to 7 will change the left most day of the calendar to Sunday. 
3) Save the file and then run the CAD Tool found in the \Schneider Electric\IONEEM\bin folder to recompile the web site. 

NOTE: It is possible that this setting may be overwritten (back to default) by future Cumulative Updates. Also, this setting only affects the calendar view in the Trend Analysis page. 
 
Was this helpful?
What can we do to improve the information ?