Technical FAQs

Ask a Question

Where are the Industry Canada certificate number of the ION8650 modem?

Issue
The ION8650 meter doesn't have a label displaying IC (Industry Canda) certification number of the internal modem. 

Product Line
ION8650

Resolution
The Industry Canada label on the meter is the same as the FCC Compliance number for the modem.
It is printed on the side of the meter and has a product identifier in the following format: US: AAAEQ##TXXXX.
For example FCC Registration Number: US: DHUMM05B8650.
Was this helpful?
What can we do to improve the information ?