Technical FAQs

Ask a Question

Does the READ_REG function block have a fixed timeout for no communications when used with the Quantum system?

Yes... The READ_REG function block has a fixed timeout of 30 seconds, When the client does not respond the timeout timer is started. If during this time period the READ_REG status does not change. An error value of 16#5055 (no network resources) is reported. We recommend the use of the MBP_MSTR function block over the READ_REG for the Quantum systems because the READ_REG doesn't have a timeout or abort pin setting.
Was this helpful?
What can we do to improve the information ?