Technical FAQs

Ask a Question

9013FSG - FSG2N technical data; how to replace it after 2013

FSG2N pressure switch for water pumping, in class 9013, is an obsolete reference in 2016. It is based on the standard FSG2 pressure switch, with the following special specifications : IP55 (instead of IP20), supplied with cable glands Pg11 in a separate package. See attached picture showing such marking. Replacement by the FSG2NE pressure switch which is IP65, supplied with 2 electrical entries incorporating Pg 13.5 plastic cable gland. See corresponding data sheet in attachment.
Was this helpful?
What can we do to improve the information ?