Technical FAQs

Ask a Question

Vijeo Designer Project won't build and shows error: Please check you Driver/Device configuration or variable settings

This error occurs if one of your variable's device address is incorrectly entered or if you recently imported variables via a Microsoft Excel modified CSV. If any of the device addresses begin with a 0, Microsoft Excel will remove those leading 0's when the CSV is saved. When you import this CSV file, Vijeo Designer does not notice that the 0 is missing and only takes the numeric value as is. Ex. Modbus address 00123 becomes 123 after Microsoft Excel saves the CSV file. This in return is an invalid address when it comes to build time of the project.
Was this helpful?
What can we do to improve the information ?