Technical FAQs

Ask a Question

EEM 5.0 - "You do not have permission to grant access to this item" when sharing trends

Issue:
When attempting to share trends following error is given: "You do not have permission to grand access to this item"


Product Line:
ION EEM 5.0

Environment:
Trend Analysis
Internet Explorer 11

Cause:
The issue has to do with compatibility issues specific to Internet Explorer 11.

Resolution:
Enable the Compatibility View within Internet Explorer and add the ION EEM website to the list of compatible sites. 
The other option would be to use a different browser such as Chrome or Firefox. 
Was this helpful?
What can we do to improve the information ?