Technical FAQs

Ask a Question

EM4200 SE Driver for PME 8.0

Issue
When adding an EM4200 meter to PME via Management Console, the Device Type selection does not include EM4200.

Product Line
Power Monitoring Expert 8.0 (PME 8.0)

Environment
Download and Install EM4200 Driver Standard Edition driver which supports all features including onboard logs, waveforms, control operation etc (provided such features are supported by the device)

Cause
PME 8.0 requires a Driver Installation for the EM4200 Series meter.

Resolution
There is a Standard Edition EM4200 Driver for PME 8.0 that will need to be installed.  

The package contains the following:
(1) Installation file (.exe)
(2) Release Notes documents (.pdf)
(3) Mapping Details / Register List (.xlsx)

Download package available at the following location:
EM4200 SE 8.0.15286.01 ENG.zip - Box

Download package is also available as an attachment below:
Was this helpful?
What can we do to improve the information ?