Technical FAQs

Ask a Question

Does HMIDID73DTD1 iDisplay support Windows Server 2008?

Issue:
Does HMIDID73DTD1 iDisplay support Windows Server 2008?

Product Line:
HMIDID73DTD1, iDisplay, Windows Server

Environment:


Cause:


Resolution:
HMIDID73DTD1 will work with Windows Server but only in single mode touch like a mouse device and install of the Windows 7 touch drivers.
Windows server OS does not support the multi touch.
Was this helpful?
What can we do to improve the information ?