Technical FAQs

Ask a Question

Does Schneider Electric offer a direct replacement for Lexium Integrated Drive type ILE1B662S2178

The Lexium Integrated Drive type ILE1B662S2178 is an OEM specific model and is not available from Schneider Electric.
Model ILE1B662S2178 is proprietary to the OEM machine builder and spares can only be attained from the OEM machine builder.

Schneider Electric does not offer a suitable replacement from our catalog that is the electrical and mechanical equivalent.

Was this helpful?
What can we do to improve the information ?