Technical FAQs

Ask a Question

Which SD card is delivered with a purchase of an M340 BMXP34xxxx CPU?

The M340 8 Meg SD card part# BMXRMS008MP is delivered with the purchase of every M340 BMXP34xxxx processor.

Functionality:
  • Application backup
  • Web server activation on the embedded Ethernet port (Transparent Ready class B)
Was this helpful?
What can we do to improve the information ?