Technical FAQs

Ask a Question

What is the maximum number of characters you can have in the alarm email body of Vijeo Designer or Magelis?

Issue:
What is the maximum number of characters you can have in the email body of Vijeo Designer or Magelis?

Product Line:
Alarm email, max characters, email truncated

Environment:


Cause:


Resolution:
The body of the Alarm email can have up to 1000 characters.  If the messages are too long, it will get truncated.  
Two options as a work around:
1 - Limit what to display in the email by removing some of the Alarm summary columns that is not required.
2 - Save the Alarms using the control variable and send the Alarm as an attachment instead.
 
Was this helpful?
What can we do to improve the information ?