Technical FAQs

Ask a Question

What is the recommended replacement for MPCNB50NAN00N Magelis iDisplay?

Issue:
What is the recommended replacement for MPCNB50NAN00N Magelis iDisplay?

Product Line:
MPCNB50NAN00N

Environment:


Cause:


Resolution:
The recommended replacement is HMIDID73DTD1.  The replacement is a touchscreen but does not have an onboard keyboard.  
Also the cutout dimensions are different and an adapter plate will be needed to mount in the existing cutout.
Was this helpful?
What can we do to improve the information ?