Technical FAQs

Ask a Question

Osisense XC - Adapted ZCKY13S89 roller lever data sheet

The adapted ZCKY13S89 roller lever data sheet is based on the standard ZCKY13 steel roller lever. The adaptation consists of punching the centre of the axle in order to avoid the loosening of the nut. Please look at the picture showing the concerned axle.

Was this helpful?
What can we do to improve the information ?