Technical FAQs

Ask a Question

Osisense XC - Special lever kit ZCKY1436202 definition

The ZCKY1436202 reference is a special lever kit based on the ZCKY45 plastic roller lever, not mounted, with 2 additional fixing washers dia 5mm and dia 6mm.

                        
Was this helpful?
What can we do to improve the information ?