Technical FAQs

Ask a Question

What is the Schneider Electric replacement for gearbox GBX0400050551F ?

The GBX0400050051F is a 40mm gearbox with a ratio of 5:1 for use with BSH0551 type motors.

This combination is no longer approved due to the possibility of breakage of the gearbox because the BSH0551 size motor torque may meet or exceed the maximum rating of this small 40mm gearbox 

The recommended replacement is as follows.

Gearbox GBX60005K = 60mm gearbox at 5:1 ratio
Mounting adapter kit GBK0600550S

See attached product data sheets
Was this helpful?
What can we do to improve the information ?