Technical FAQs

Ask a Question

Osisense XC - Datasheet of the adapted lever ZCKY13S83

Please find attached the datasheet of the adapted lever ZCKY13S83. Difference with the standard ZCKY13 is the roller diameter (35mm instead of 22mm). Such adapted lever is not available in stock.
Was this helpful?
What can we do to improve the information ?