Technical FAQs

Ask a Question

What are the torque specification for the Quantum field wire connectors, 140XTS02000 ?

Below is the torque specification for both the (2) connector block mounting screws as well a the field wiring connectors.

         Typical             Maximum

            0.6                      1.13     Nm

            5.4                      10.0     in-lbs



R-71117
Was this helpful?
What can we do to improve the information ?