Technical FAQs

Ask a Question

Osisense XM_Adapted pressure switch XMLCS04B2S12SB5 datasheet

The XMLCS04B2S12SB5 is an adapted pressure switch based on the standard XMLCS04B2S12 30bar overpressure, with some pressure adjustement made in production plant. Please find attached the XMLCS04B2S12SB5 datasheet, origin Sensors Adaptation Centre in France, giving the adjusted pressure values (PH=1.2 PB=1.0 bar). Please note that the XMLCS04B2S12SB5 reference sales are reserved to the german OEM who asked for.
Was this helpful?
What can we do to improve the information ?