Technical FAQs

Ask a Question

What are the system requirements for SoSafe configurable software?

SoSafe Configurable software runs on PC with:
 
> RAM: 256 MB
> Hard disk: free space > 300 MB
> USB connector: 1.1 or 2.0

> Microsoft Windows® XP SP3 (service Pack 3) / Vista 32-bit,
> Microsoft Windows® 7 32 and 64-bit ,
> Microsoft Windows® 8.1 32 and 64-bit
> Microsoft Framework 3.5 (or higher).
Was this helpful?
What can we do to improve the information ?