Technical FAQs

Ask a Question

Where do I find CAD drawings for Lexium Integrated Drives?

CAD files are hosted by

Click on "To Overview", then navigate to Schneider Electric Motion
Choose "Integrated Compact Drives"
Next select whether you have a servo, stepper or brushless dc type
Clicking on the base model that is provided will allow you to modify the configuration of the model to match they type you are looking for.

Note that you must create a free account to proceed with CAD file creation.
Was this helpful?
What can we do to improve the information ?