Technical FAQs

Ask a Question

How can the username and password be reset to default on the 140NWM10000 if the passord is lost?

 
Goals and Symptoms
How can the username and password be reset to default on the 140NWM10000 if the passord is lost?

Facts and Change
140NWM10000

Causes and Fixes 
Due to Cyber Security reasons, the module must be sent back to the factory for repair in order to restore the
username and password back to the default setting..
Was this helpful?
What can we do to improve the information ?