Technical FAQs

Ask a Question

Can the XPSMCM non-safe communications module be configured next to the Safety controller?

Issue:
Can the XPSMCM non-safe communications module be configured next to the Safety controller?

Product Line:
XPSMCMCO0000CO, XPSMCMCO0000DN, XPSMCMCO0000EC, XPSMCMCO0000EI, XPSMCMCO0000EM, XPSMCMCO0000EP, 
XPSMCMCO0000MB, XPSMCMCO0000PB, XPSMCMCO0000UB, XPSMCM

Environment:


Cause:


Resolution:
The non-safe communication modules need to be at the end of the rack.  It can not be next to the controller.
Was this helpful?
What can we do to improve the information ?