Technical FAQs

Ask a Question

Osisense XC - IP degree of protection of the XC1ZP* snap switches

For our old XC1ZP* snap switches, the degree of protection is IP30, according to the IEC 60529 standard.

Was this helpful?
What can we do to improve the information ?