Technical FAQs

Ask a Question

Osisense XM - What is the diameter of the cable with fitting for the XL1 float switches

For the old XL1 float switches, the diameter of the cable with fitting is the following :
- polyester (ZL1AB106 & ZL1AB1012) : dia 6mm
- stainless steel (ZL1AB116 & ZL1AB1112) : dia 2mm.
They are used in the XL1 models with cable.

Was this helpful?
What can we do to improve the information ?