Technical FAQs

Ask a Question

What is the DHCP rolename of a BMXPRA0100 when using the rotary switches?

Title
The DHCP rolename of a BMXPRA0100
 
Issue
The DHCP rolename of a BMXPRA0100 when using the rotary switches.
 
Product Line
M340 BMXPRA0100
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
For the M340 BMXPRA0100 the DHCP name used when using the rotary swtich settings is BMX_0100_xxy.
The numeric value between 00 and 159 set on the rotary switches. For the default device name, xx is the value of the upper rotary switch and y is the value of the lower rotary switch.
Was this helpful?
What can we do to improve the information ?