Technical FAQs

Ask a Question

Preventa XU - Which Thesys contactors to associate with a safety light curtain XUSL4E or XUSL2E to reach SIL3 or PLe category 4, in a standalone mode?

Please find attached a document explaining
- what is an XUSL4E-2E standalone solution,
- which Thesys contactors to select in such solution,
- which Thesys accessory to use in the contactors to identifiy them when they are used in a safety chain solution.
Was this helpful?
What can we do to improve the information ?