Technical FAQs

Ask a Question

Does the CPU M580 log an event when there is a hardware change (module replacement,n or SD card removal) ?

No, events related to physical access to the system, are not logged.
Was this helpful?
What can we do to improve the information ?