Technical FAQs

Ask a Question

Preventa XY2C - XY2CH33010 rope pull switch datasheet

Please find attached the XY2CH33010 datasheet available on "" site (@
Such product is not suitable for an E.stop function, complying to the safety standards like the ISO 13850.... It does not have any locking function of the cable actuation, so no reset button in the front cover. Colour is the blue one. It is considered as a simple stop. Such product version does not appear in our E.stop rope pull switches catalogue (Preventa XY2C). It is not UL NISD certified.
Was this helpful?
What can we do to improve the information ?