Technical FAQs

Ask a Question

Why do I get a "The entered Customer information is incomplete" after filling out the Customer Information form in SoSafe Configurable version 1.5078

The use of any non alpha numeric character in any of the fields of this form will generate this error. For example, entering customer name such as Seamus O'Connor will generate this error because the surname O'Connor contains an apostrophe. If you enter the name as OConnor, the instalation program accepts the information and the installation will continue.

Was this helpful?
What can we do to improve the information ?