Technical FAQs

Ask a Question

Why does Icla Easy ask for an EDS file when I attempt to connect to my Lexium Integrated Drive?

Icla easy is an older version of commissioning software that was developed by Berger Lahr to support there ICLA motors.
The Icla easy software was replaced by Lexium CT software and Icla Easy is no longer supported.
Because of this customers that use Icla easy will find that new Lexium Integrated Drives with newer firmware are not supported by Icla easy and the  software will request an additional EDS file.

Customers should upgrade to Lexium CT commissioning software.
Lexium CT supports all versions of firmware from the oldest to the most recent and will replace Icla easy so Icla easy can be removed after installing Lexium CT

 
Was this helpful?
What can we do to improve the information ?