Technical FAQs

Ask a Question

Osisense XC - what is the XCKN2118P20S98 limit switch

The XCKN2118P20S98 limit switch is an adapted switch created for a customer. It is in fact the XCKN2118P20 limit switch (standard reference) with lever arm turned of 90° on the right and roller turned internally. So corresponding data sheet is the same as the standard switch XCKN2118P20, available at the following @
http://www.tesensors.com/us/en/product/limit-switches/xc-standard/?el_typ=product&cat_id=BU_AUT_520_L4&conf=basket&prd_id=XCKN2118P20&scp_id=Z000&lc=en&s_typ=guided_aut
Was this helpful?
What can we do to improve the information ?