Technical FAQs

Ask a Question

How woks the anti-condensation valve NSYCAG12LPH from Schneider-electric Universal Enclosures offer

The function of this valve is to balance the air pressure between the interior and outside the enclosure. Particularly when the inner and out temperatures are different. When air pressure inside and outside is equal, condensation inside the enclosure is avoided.

For the functional principle see attached file.
 
Was this helpful?
What can we do to improve the information ?