Technical FAQs

Ask a Question

Osisense XC - What is the XCKL808141 part number ? How to order it ?

The XCKL808141 part number is not a valid reference to order. 808141 is the image number of the XCKL product shown into the "Osisense XC limit switches" catalogue. Please see attached picture. Such ID number appears in the net search when the link is associated to our catalogue page. To select the right reference(s) to order, please check on the contact body the ZCKL reference and on the head the ZCKD reference to order either a complete XCKL reference, either the sub-assemblies body+head+lever arm if it exists. See attached catalogue page giving complete switch references.

Was this helpful?
What can we do to improve the information ?