Technical FAQs

Ask a Question

Error in MiCOM S1 Studio Not Supported when using quick connect.

When trying use the quick connect in MiCOM S1 Studio a Not Supported error appears beside the data model number. 

Product Line  
MiCOM S1 Studio

Connecting to MiCOM relays

The MiCOM data model that is being connected to is not on the computer that is being used.

The first step will be to download the data model from Data Model Manager.  The instructions are in the follow article FA221295
Once the data model is download try the quick connect again.   The model will now not have the not supported error.

Note: That if a password is asked for the default is AAAA password unless changed in MiCOM S1 Studio

Was this helpful?
What can we do to improve the information ?