Technical FAQs

Ask a Question

Instructions on How to Migrate PME 7.2 System to a New Server

Issue
Migrating a PME 7.2 system to a new server.

Product Line
Power Monitoring Expert 7.2

Environment
Standalone System

Cause 
The system needs to be fully moved to a new server keeping all the configuration, set up and data intact

Resolution
*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system. Always backup the registry before making any changes.* 
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.* 


See the attached document for instructions on how to migrate a PME 7.2 system to a new server.
Was this helpful?
What can we do to improve the information ?