Technical FAQs

Ask a Question

What is the part number for the 24 pin C1 connector on the signal cables VW3S8201Rxx used with the SD326 drives?

Question:
What is the part number for the 24 pin C1 connector on the signal cables VW3S8201Rxx used with the SD32x drives?

Answer:

Issue: Part number of sub-assembly

Product Line: Lexium SD3

Environment: None

Cause:

Resolution:

The part number of the conector and the crimp tool and the manufacturer information are provided below.

This information can be found in the installation section of the SD326 user manual.



 
Was this helpful?
What can we do to improve the information ?