Technical FAQs

Ask a Question

Which Magelis targets can use the battery part number, HMIZGBAT?

Issue:
Which Magelis targets can use the battery part number, HMIZGBAT?

Product Line:
backup battery, HMIGTO, HMIGTU

Environment:


Cause:


Resolution:
That battery is for the Magelis HMIGTO series except HMIGTO1300 / 1310 / 2300.
Was this helpful?
What can we do to improve the information ?