Technical FAQs

Ask a Question

Task Scheduler Error “A specified logon session does not exist” when trying to manually create a Windows scheduled task

Issue 
When the PME installer does not create the Windows scheduled tasks, you can manually install the scheduled tasks.  Sometimes, importing tasks gives you the following error:

Error message: An error has occurred for MYTASK. Error message: The following error was reported: A specified logon session does not exist. It may already have been terminated..


Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment
PME/PME4HC/PME4DC Installation

Cause
The local policy "Network access: Do not allow storage of passwords and credentials for network authentication" domain security policies blocks the creation of Windows scheduled tasks with security options "Run whether user is logged on or not"

Resolution

Setting the Network access: Do not allow storage of passwords and credentials for network authentication policy to Disabled.  Please refer to the below images.

1.  Open the Windows Local Group Policy Editor by pressing the windows key and typing "SECPOL.MSC"
2.  Once there, navigate to Security Settings > Local Policies > Security Options.  



3.  Once there, find the Network access: Do not allow storage of passwords and credentials for network authentication policy and double click it and set the policy to Disabled in the Local Security Setting tab and click OK.



4. Once the above local security policy has been disabled, you will be able to manually create tasks in Windows Task Scheduler.

 
Was this helpful?
What can we do to improve the information ?