Technical FAQs

Ask a Question

What is the replacement for the Advantys STBDDO3410 digital output module?

The replacement is the STBDDO3410K. The "K" at the end of the part number designates kit. The kit now contains the following parts:
One STBDDO3410 digital output module
One STBXBA1000 base
Two STBXTS1100 6-terminal screw type connectors
Two STBXTS2100 6-terminal spring clamp connectors
Was this helpful?
What can we do to improve the information ?