Technical FAQs

Ask a Question

What temperature standard does the BMXART0414 or BMXART0814 follow when used use with platinum RTD ?

Each of these modules use the IEC 751-1995 standard for both Pt100 & Pt1000. These modules also comply with the Japanese Industrial Standard  JIS C 1604-1997.
Was this helpful?
What can we do to improve the information ?